OMRON to Release Redesigned E5GN, Smallest Member of Bestselling E5_N Series of Temperature Controllers
- Print Help
- Change Text Size
- October 1, 2009
- FOR IMMEDIATE RELEASE
Tokyo, Japan – OMRON Corporation (TOKYO: 6645, ADR: OMRNY) today launched the redesigned E5GN temperature controller, the smallest controller (DIN 48 x 24 mm) in the bestselling E5_N series of temperature controllers, to global markets. 1 <Images>
Since the E5_N series was first introduced in 1998, the line-up has retained its fundamental strengths, while product features have evolved in response to the needs of our onsite customers. The series has achieved worldwide sales of three million units to date.
The E5_N series was developed around the concept of "onsite simplicity." It features easy model selection, operation and maintenance, which are crucial to achieving smooth onsite operations.
The E5GN features a display that reliably notifies the operator of current conditions, various functions that reduce the time required for settings and adjustments, reliable designs that reduce maintenance, and various services all aimed at ensuring simplicity in temperature control for all production sites.
The E5_N series comprises two functional variations: basic models that provide excellent cost/performance and general applicability, and advanced models for applications that require superior performance and functionality.
The E5GN released today is a basic model. Adopting the "onsite simplicity" concept of the series, its compact size of DIN 48 x 24 mm allows for flexibility in installation locations.
With the addition of the compact G size (DIN 48 x 24 mm), the E5—N series now provides a selection of four sizes, also including the A size (DIN 96 x 96 mm), E size (DIN 48 x 96 mm) and C size (DIN 48 x 48 mm), allowing customers to select the best model for the application site.
1 The E5GN was released to the Japanese market on September 1.
Features
Readability
- The PV display color can be changed to show the current display status through color variations.
- PV/SV status displays enable showing alarms and other status with textural information.
Easy Operation
- Screwless clamp terminals have been used to reduce wiring work.
- The parameter mask function of the CX-Thermo support software can be used to hide unnecessary parameters to prevent setting errors and inadvertent operation. (CX-Thermo version 4.2 or higher is required for the E5GN.)
- All models are equipped with a support software port on the side of the unit to enable connecting to the CX-Thermo (sold separately) for easy setting and adjustment.
Easy Model Selection
Universal inputs that allow either thermocouples or platinum resistance thermometers to be connected to the same temperature controller help reduce stock quantities.
Easy Maintenance
A control output ON/OFF counter notifies the user of the maintenance cycle for internal and external relays.
Improvements over the Previous E5GN
- Increased indication accuracy from ±0.5% PV to ±0.3% for thermocouples and ±0.2% PV for platinum resistance thermometers
- Improved the sampling cycle from 500 ms to 250 ms
- Added specifications for analog inputs
- Added specifications for current outputs
- Added specifications for loop burnout detection
- Added specifications for heater overcurrent alarms
- Added specifications for RS-232C communications
- Added specifications for two independent alarms
Sales Target
40,000 units/year
Main Applications
Inspection devices, control panels, semiconductor manufacturing equipment, food processing equipment, packaging machines, conveyance equipment, scientific devices
Production Site
OMRON (Shanghai) Co., Ltd.
Release Date
October 1, 2009 (global)
For more information, visit the E5GN product page on OMRON IA's global website at http://www.ia.omron.com/product/family/1434/index_fea.html
About OMRON
Headquartered in Kyoto, Japan, OMRON Corporation is a global leader in the field of automation. Established in 1933 and headed by President & CEO Hisao Sakuta, OMRON has over 32,000 employees in 38 countries working to provide products and services to customers in a variety of fields, including industrial automation, electronic components, social systems (ticket gate machines, ticket vending machines and traffic control) and healthcare. For more information, visit OMRON's website at www.omron.com.
- Media Inquires
- Osamu Harasawa (osamu_harasawa@omron.co.jp)
OMRON IA Strategy Planning Division
Tel.: +81-3-3779-9434